Ping not working in RT1024 custom board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Ping not working in RT1024 custom board

跳至解决方案
1,853 次查看
sbabu
Contributor III

Hi All,

We are testing our ethernet interface(lwip ping demo example) on our custom board based out of MIMXRT1024 and PHY is KSZ8081RND. The ping is working fine in EVAL kit but not working in our board. The Link is coming up only if we disable autoNeg but tx and rx not happening. Any pointers will be appreciated.

Thanks.

Babu

0 项奖励
回复
1 解答
1,804 次查看
sbabu
Contributor III

@PabloAvalos Hi Pablo, Thanks. We got the Enet working but we are having issue in brining up the SC Card on RT1024. The SD_ApplicationSendOperationCondition() command is failing from the MCUXpresso demo example. We are not able to get command response and its stuck waiting for command response. Please let me know your team thoughts on this.

 

Thanks,

Subash

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,823 次查看
PabloAvalos
NXP TechSupport
NXP TechSupport

Dear @sbabu 

 

Thanks a lot for reaching our technical support and for your patience.

 

Regarding your issue, I would like to help, but first I would like to know if you are following the Hardware Design Guide for your custom board, because as you mentioned, on EVAL board it is working fine, so then you will need to check your hardware connections and if everything seems ok regarding the HUG (Hardware User Guide) and the connection are similar to the EVK board.

 

Hope you may have the connection well, please let me know if you find something.

 

BR.
Pablo Avalos.

0 项奖励
回复
1,805 次查看
sbabu
Contributor III

@PabloAvalos Hi Pablo, Thanks. We got the Enet working but we are having issue in brining up the SC Card on RT1024. The SD_ApplicationSendOperationCondition() command is failing from the MCUXpresso demo example. We are not able to get command response and its stuck waiting for command response. Please let me know your team thoughts on this.

 

Thanks,

Subash

0 项奖励
回复
1,781 次查看
PabloAvalos
NXP TechSupport
NXP TechSupport

Dear @sbabu 

 

Thanks a lot for response.

 

Regarding the issue, I do not have the exact clue on what's going on, but I am wondering if you have already tried to run the sdcard freertos example from SDK to try to read/write your SD and avoid the errors?

Here is a capture of the readme file so you can make sure to follow all the steps to run the demo and see if it is not a hardware issue.

2023-05-30_14-02-41 RW SDCARD FREERTOS README FILE RT1024.png

 

Please let me know if this demo runs successfully on your board to discard HW issues.

 

Thanks a lot.
BR.
Pablo Avalos. 

0 项奖励
回复