Packing information about MIMX8QM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Packing information about MIMX8QM

1,723件の閲覧回数
eric_hong
Contributor II

Hi,

Would anyone help to provide document with packing information of i.MX 8QM?

Regards,

Eric 

0 件の賞賛
返信
3 返答(返信)

1,698件の閲覧回数
brian14
NXP TechSupport
NXP TechSupport

Hi @eric_hong, 

Based on the iMX8QM datasheet the processor package is a FCPBGA 29mmx29mm.
Here is more information from the package.

BGA1313, ball grid array package, 1313 terminals, 0.75 mm pitch, 29 mm x 29 mm x 2.37 mm body (nxp.c...

Tell me if you need any specific information about this package.

Have a great day!

0 件の賞賛
返信

1,680件の閲覧回数
tw_wang
Contributor I

Hi Brian

Thank you!  But we also need packing document regarding  tray or reel information to the  iMX8QM, FCPBGA 29mmx29mm.

Regards,

TW Wang

 

 

0 件の賞賛
返信

1,661件の閲覧回数
brian14
NXP TechSupport
NXP TechSupport


Hi @tw_wang, 

For this documentation, please require a ticket on the following link:

Brian_Ibarra_0-1692299809112.png

 

Support | NXP Semiconductors

Thank you and have a great day!

0 件の賞賛
返信