Packing information about MIMX8QM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Packing information about MIMX8QM

1,684 次查看
eric_hong
Contributor II

Hi,

Would anyone help to provide document with packing information of i.MX 8QM?

Regards,

Eric 

0 项奖励
回复
3 回复数

1,659 次查看
brian14
NXP TechSupport
NXP TechSupport

Hi @eric_hong, 

Based on the iMX8QM datasheet the processor package is a FCPBGA 29mmx29mm.
Here is more information from the package.

BGA1313, ball grid array package, 1313 terminals, 0.75 mm pitch, 29 mm x 29 mm x 2.37 mm body (nxp.c...

Tell me if you need any specific information about this package.

Have a great day!

0 项奖励
回复

1,641 次查看
tw_wang
Contributor I

Hi Brian

Thank you!  But we also need packing document regarding  tray or reel information to the  iMX8QM, FCPBGA 29mmx29mm.

Regards,

TW Wang

 

 

0 项奖励
回复

1,622 次查看
brian14
NXP TechSupport
NXP TechSupport


Hi @tw_wang, 

For this documentation, please require a ticket on the following link:

Brian_Ibarra_0-1692299809112.png

 

Support | NXP Semiconductors

Thank you and have a great day!

0 项奖励
回复