PF0100 Linear Regulator Inputs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PF0100 Linear Regulator Inputs

跳至解决方案
1,280 次查看
atillametetured
Contributor V

Greetings,

Are we able to supply the linear regulators from an outer source apart from the inner Switching Regulators or the Vin of the IC? Anywhere I looked its the other way around and I cant figure out if thats so because its a good practice or a must?

Best Regards,

Mete

标签 (1)
标记 (5)
0 项奖励
回复
1 解答
1,119 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Atilla

yes it is possible to supply the linear regulators from an outer sources

apart from the inner Switching Regulators or the Vin.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,120 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Atilla

yes it is possible to supply the linear regulators from an outer sources

apart from the inner Switching Regulators or the Vin.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------