PF0100 Linear Regulator Inputs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF0100 Linear Regulator Inputs

Jump to solution
1,277 Views
atillametetured
Contributor V

Greetings,

Are we able to supply the linear regulators from an outer source apart from the inner Switching Regulators or the Vin of the IC? Anywhere I looked its the other way around and I cant figure out if thats so because its a good practice or a must?

Best Regards,

Mete

Labels (1)
0 Kudos
Reply
1 Solution
1,116 Views
igorpadykov
NXP Employee
NXP Employee

Hi Atilla

yes it is possible to supply the linear regulators from an outer sources

apart from the inner Switching Regulators or the Vin.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,117 Views
igorpadykov
NXP Employee
NXP Employee

Hi Atilla

yes it is possible to supply the linear regulators from an outer sources

apart from the inner Switching Regulators or the Vin.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------