PF0100 Linear Regulator Inputs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF0100 Linear Regulator Inputs

ソリューションへジャンプ
1,750件の閲覧回数
atillametetured
Contributor V

Greetings,

Are we able to supply the linear regulators from an outer source apart from the inner Switching Regulators or the Vin of the IC? Anywhere I looked its the other way around and I cant figure out if thats so because its a good practice or a must?

Best Regards,

Mete

ラベル(1)
0 件の賞賛
返信
1 解決策
1,589件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Atilla

yes it is possible to supply the linear regulators from an outer sources

apart from the inner Switching Regulators or the Vin.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,590件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Atilla

yes it is possible to supply the linear regulators from an outer sources

apart from the inner Switching Regulators or the Vin.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------