PCIe clock cannot be enabled

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCIe clock cannot be enabled

1,361件の閲覧回数
增超段
Contributor I

problem:

PCIe clock cannot be enabled, clock pins have no signal when kernel booting 

project details: imx6 android4.4 linux 3.0.35_B01_V1.0 

log : 

[ 6.459812] iMX6 PCIe PCIe RC mode imx_pcie_pltfm_probe entering.
[ 6.579052] PCIE: imx_pcie_pltfm_probe start link up.
[ 7.189979] link up failed, DB_R0:0x0047b000, DB_R1:0x08200000!
[ 7.195994] IMX PCIe port: link down with power supply 1!

 more kernel logs blow this context

0 件の賞賛
返信
1 返信

1,271件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 增超 段 

one can test pcie with baremetal sdk tests, it can be found

on SMP Enable in IMX6 

check hardware using i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信