I would like to test the function of the tamper pins on this board. My Project is about detecting a tamper attempt on a case which is going to be built around the board. For my prototype I wanted to show that if I cut a wire (which is attached to the board) the IMX6-Board can detect this.
Is this possible?
If yes, where do I connect the wire?
Can I connect the wire to the tamper Pins (e.g. SNVS_Tamper0 and SNVS_Tamper1)?
Which registers do I have to enable?
Thanks for the help.
Hi Imme
there is no tamper pin function in i.MX6ULL. TAMPER0-9 are used as GPIO.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------