PCF85263A RTC Linux driver for i.mx6ul

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCF85263A RTC Linux driver for i.mx6ul

3,200件の閲覧回数
dhvanil_patel1
Senior Contributor I

Hi,

I am using an external  PCF85263A  RTC on I2C interface of i.MX6ul.

I need linux based RTC driver for PCF85263A .

Can you please share the RTC driver with me ? I need it in very urgency.

-

Dhvanil Patel

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

2,610件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Dhvanil

please look at examples of pcf852x driver in

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/boot/dts/imx6qdl-cubox-i.d...

https://forums.xilinx.com/t5/Embedded-Linux/RTC-support-on-the-Zynq/td-p/391717

Unfortunately I am not aware of PCF85263A usage with i.MX6UL.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,610件の閲覧回数
dhvanil_patel1
Senior Contributor I

Hi igor,

I checked the RTC driver in kernel. but this RTC driver is for PCF8523 and We are using PCF8526A. These both ICs are having different I2C register map. So I am not able to use this driver.

Can you please point out the proper RTC driver for  PCF8526A ?

-

Dhvanil Patel

0 件の賞賛
返信

2,610件の閲覧回数
dhvanil_patel1
Senior Contributor I

Hi igor,

Thank you for your response.

We want to increase battery coin cell life by using external RTC on im6ul.

Please let us share your thought regarding external RTC.  Is it worthful to use external RTC or not   ?

-

Regards,

Dhvanil Patel

0 件の賞賛
返信