how many trustzone tech used in i.MX6DL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how many trustzone tech used in i.MX6DL

1,920件の閲覧回数
qingxiangluo
Contributor I

Refer to the user's manual of i.MX6DL:

Document Number: IMX6SDLRM

Rev. 1, 04/2013

and just find some words for trustzone, so i want to know how many TZ IP/tech is used in i.MX6DL?

like TZPC,TZASC? or whether NXP has special document for trustzone related topics?

in the bootloader, whether it already support trustzone feature?

thanks!

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,608件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi qingxiang

security features are described in Security Manual attached on

Q&A: How is mx6 PMIC_ON_REQ under SW control? | NXP Community

secure boot on application note AN4581

http://www.nxp.com/files/32bit/doc/app_note/AN4581.pdf

for TrustZone one can use arm resources:

TrustZone - ARM

https://www.sbs.ox.ac.uk/cybersecurity-capacity/system/files/ARM%20Security%20Technology.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,609件の閲覧回数
qingxiangluo
Contributor I

Hello igor,

          To use TZ technology, is it possible to separate GPU 2D/3D to different world? like 2D for secure while 3D for Non-secure?

how?

0 件の賞賛
返信