OCOTP Memory Map/Register Definition

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OCOTP Memory Map/Register Definition

Jump to solution
26,502 Views
andreacelani
Contributor II

I have questions about the chapter "6.3.5 OCOTP Memory Map/Register Definition" (page 1387) in the IMX8M owner manual (IMX8MDQLQRM, Rev. 0, 01/2018).  I am not sure, but I have found are some errors in the Bank/Word assignment of some OCOTP fuse:

1.

About Field Return

3035_0630 Value of OTP Bank5 Word6 (Field Return)

(Question) It think it should be

3035_0630 Value of OTP Bank8 Word3 (Field Return)

2.

From OCOTP Address  3035_0820

all Bank and Word have the same value

Value of OTP Bank16 Word0 (or)

Value of OTP Bank17 Word0

(Question) I think this is a bug of the manual.

 

So, is there an official IMX8M document that contains the correct Bank/Word value for the OCOTP memory map? Is there a new version of IMX8M owner manual with corrected OCOTP memory map?

Labels (1)
1 Solution
2,405 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

   Indeed there were some mistakes in this RM according to fuse mapping,

thanks you for noticing us, it will be fixed as soon as possible.

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

View solution in original post

1 Reply
2,405 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

   Indeed there were some mistakes in this RM according to fuse mapping,

thanks you for noticing us, it will be fixed as soon as possible.

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!