OCOTP Memory Map/Register Definition

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OCOTP Memory Map/Register Definition

ソリューションへジャンプ
26,427件の閲覧回数
andreacelani
Contributor II

I have questions about the chapter "6.3.5 OCOTP Memory Map/Register Definition" (page 1387) in the IMX8M owner manual (IMX8MDQLQRM, Rev. 0, 01/2018).  I am not sure, but I have found are some errors in the Bank/Word assignment of some OCOTP fuse:

1.

About Field Return

3035_0630 Value of OTP Bank5 Word6 (Field Return)

(Question) It think it should be

3035_0630 Value of OTP Bank8 Word3 (Field Return)

2.

From OCOTP Address  3035_0820

all Bank and Word have the same value

Value of OTP Bank16 Word0 (or)

Value of OTP Bank17 Word0

(Question) I think this is a bug of the manual.

 

So, is there an official IMX8M document that contains the correct Bank/Word value for the OCOTP memory map? Is there a new version of IMX8M owner manual with corrected OCOTP memory map?

ラベル(1)
1 解決策
2,330件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

   Indeed there were some mistakes in this RM according to fuse mapping,

thanks you for noticing us, it will be fixed as soon as possible.

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

元の投稿で解決策を見る

1 返信
2,331件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

   Indeed there were some mistakes in this RM according to fuse mapping,

thanks you for noticing us, it will be fixed as soon as possible.

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!