Hi,
1. I have just received a baseline SABRE-SD board which came with Android SD Card and it worksI
2. I have Ubuntu 14.04 LTS (with all the regular updates) Guest OS within VMWare Workstation Pro 12.0 environment
3. I have retrieved the Yocto source based upon source retrieved from here:
4. I built this using Using the default setup line:
      source setup-environment build
      bitbake core-image-minimal
5. a sdcard image was built:
core-image-minimal-imx6qsabresd.sdcard.gz
6. I flashed the SD Card (note: in my setup the SD Card is /dev/sda)
sudo dd if=core-image-minimal-imx6qsabresd.sdcard of=/dev/sda bs=1M
u. I put this into the sdcard slot and try to power-up and it fails to do anything after the last line...
U-Boot 2016.07+fslc+ge6b4241 (Jan 31 2017 - 19:57:32 -0800)
CPU: Freescale i.MX6Q rev1.5 996 MHz (running at 792 MHz)
CPU: Automotive temperature grade (-40C to 125C) at 21C
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 1 GiB
PMIC: PFUZE100 ID=0x10
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment
PCI: pcie phy link never came up
auto-detected panel HDMI
Display: HDMI (1024x768)
In: serial
Out: serial
Err: serial
Net: FEC [PRIME]
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc1 is current device
reading boot.scr
** Unable to read file boot.scr **
reading zImage
6527280 bytes read in 312 ms (20 MiB/s)
Booting from mmc ...
reading imx6q-sabresd-ldo.dtb
45464 bytes read in 19 ms (2.3 MiB/s)
Kernel image @ 0x12000000 [ 0x000000 - 0x639930 ]
## Flattened Device Tree blob at 18000000
 Booting using the fdt blob at 0x18000000
 Using Device Tree in place at 18000000, end 1800e197
Starting kernel ...
Any thoughts...
tom
Thanks Igor for your reply, I was trying to build a non-ga version from scratch...
I am also not a fan of PC based tools for loading mmc cards that are directly attached to the board.
With that said, I may try building the GA version of Yocto - just to see if that goes better....
tom
I think I have more information while looking at the build/tmp/deploy/images/imx6qsabresd directory
this is the zImage that is booting:
zImage -> zImage--4.1-1.0.x+git0+2fa70a9061-r0-imx6qsabresd-20170204002511.bin
But, it is trying to load:
reading imx6q-sabresd-ldo.dtb
The fdt script is screwed up:
findfdt=if test $fdt_file = undefined; then if test $board_name = SABREAUTO && test $board_rev = MX6QP; then setenv fdt_file imx6qp-sabreauto.dtb; fi; if test $board_name = SABREAUTO && test $board_rev = MX6Q; then setenv fdt_file imx6q-sabreauto.dtb; fi; if test $board_name = SABREAUTO && test $board_rev = MX6DL; then setenv fdt_file imx6dl-sabreauto.dtb; fi; if test $board_name = SABRESD && test $board_rev = MX6QP; then setenv fdt_file imx6qp-sabresd.dtb; fi; if test $board_name = SABRESD && test $board_rev = MX6Q; then setenv fdt_file imx6q-sabresd-ldo.dtb; fi; if test $board_name = SABRESD && test $board_rev = MX6DL; then setenv fdt_file imx6dl-sabresd-ldo.dtb; fi; if test $fdt_file = undefined; then echo WARNING: Could not determine dtb to use; fi; fi;
But, there is a non-ldo dtb file in directory:
zImage-imx6q-sabresd.dtb
I think this is the right one (imx6q-sabresd.dtb)
except when I try this - it has the same failure?
ideas/thoughts?
sabreauto board can not use ldo-bypass, the reason is WDOG_B pin not connect to external PMIC.
Best regards
igor
yes - that is why I went around the fdtfind script and hard-coded the dtb to be the imx6q-sabresd.dtb.
same ending...
I think you are using the i.MX6Q sabresd board not sabreauto board (correct me if I am wrong) .
So in that case I think you don't need to hard code the dtb name in fdt script.
Thanks,
Vinod
You can check the correct dtb one from your u-boot (somewhere in include/configs/* directory). Because that is the place where you mention the dtb file name for booting.
#if defined(CONFIG_MX6Q)
#define CONFIG_DEFAULT_FDT_FILE "imx6q-sabresd-ldo.dtb"
#elif defined(CONFIG_MX6DL)
#define CONFIG_DEFAULT_FDT_FILE "imx6dl-sabresd-ldo.dtb"
One thing which is looking little wired from your logs.
reading zImage
6527280 bytes read in 312 ms (20 MiB/s)
Generally kernel image size is 4-5MB, but in your case it is somewhere near to 6.5MB. So the size of kernel image can also leads to kernel hang.
Thanks,
Vinod
re: kernel size....
I did nothing but build core-image-sato - nothing custom...
that is what it made...what do you suggest - re-configure linux kernel and disable a few things?
Yes that is my concern. You can try by disabling few of things.
Hi Thomas
one can check i.MX software resources link
and start with Linux 4.1.15_1.0.0 Demo Images
Use mfg tools for programming (for sd - mfgtool2-yocto-mx-sabresd-sdcard-sd.vbs, for emmc - mfgtool2-yocto-mx-sabresd-emmc.vbs)
or use sect.4.3.2 Copying the full SD card image attached Linux Guide from Doc package (L4.1.15_1.0.0_LINUX_DOCS)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------