Need second gpio pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,236件の閲覧回数
jimpanse
Contributor II

Hey folks,

I'm already toggling the USER led on my i.MX53 QSB via the GPIO7 register. That works pretty fine.

Now I need a second GPIO pin that i can control via software and that is (easily) accessible from

outside.

Can U help me? Thanks in advance!

ラベル(1)
タグ(3)
1 解決策
2,117件の閲覧回数
RodBorras
NXP Employee
NXP Employee

Hi,

Assuming you are not using the microphone, have you considered MIC_DET_B (PATA_DATA6=GPIO2_GPIO[6])?

Similarly, if you are not using the headset output, you could try HEADPHONE_DET_B (PATA_DATA5=GPIO2_GPIO[5]).

Regards,

Rod.

元の投稿で解決策を見る

2 返答(返信)
2,118件の閲覧回数
RodBorras
NXP Employee
NXP Employee

Hi,

Assuming you are not using the microphone, have you considered MIC_DET_B (PATA_DATA6=GPIO2_GPIO[6])?

Similarly, if you are not using the headset output, you could try HEADPHONE_DET_B (PATA_DATA5=GPIO2_GPIO[5]).

Regards,

Rod.

2,117件の閲覧回数
jimpanse
Contributor II

Thank you very much! Perfect answer!

0 件の賞賛
返信