Need second gpio pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need second gpio pin

Jump to solution
2,279 Views
jimpanse
Contributor II

Hey folks,

I'm already toggling the USER led on my i.MX53 QSB via the GPIO7 register. That works pretty fine.

Now I need a second GPIO pin that i can control via software and that is (easily) accessible from

outside.

Can U help me? Thanks in advance!

Labels (1)
Tags (3)
1 Solution
2,160 Views
RodBorras
NXP Employee
NXP Employee

Hi,

Assuming you are not using the microphone, have you considered MIC_DET_B (PATA_DATA6=GPIO2_GPIO[6])?

Similarly, if you are not using the headset output, you could try HEADPHONE_DET_B (PATA_DATA5=GPIO2_GPIO[5]).

Regards,

Rod.

View solution in original post

2 Replies
2,161 Views
RodBorras
NXP Employee
NXP Employee

Hi,

Assuming you are not using the microphone, have you considered MIC_DET_B (PATA_DATA6=GPIO2_GPIO[6])?

Similarly, if you are not using the headset output, you could try HEADPHONE_DET_B (PATA_DATA5=GPIO2_GPIO[5]).

Regards,

Rod.

2,160 Views
jimpanse
Contributor II

Thank you very much! Perfect answer!

0 Kudos
Reply