NXP i.mx8M Mini with 8GB LPDDR4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP i.mx8M Mini with 8GB LPDDR4

ソリューションへジャンプ
2,548件の閲覧回数
richard_hu
Senior Contributor I

Dear, Sir:

We have a custom i.mx8M Mini board.

we have validated 4GB LPDDR4 on it and it works fine.

Now we change the LPDDR4 from 4GB to 8GB. And we encounter some problems.

 

The DDR Register Programming Aid (RPA) we use is "MX8M_Mini_LPDDR4_RPA_v18.xlsx".

The NXP DDR tool we use is "mscale_ddr_tool _v3.20_setup.exe".

 

First, we follow the DRAM datasheet to set up device information for 8GB LPDDR4 in RPA.

i.mx8MM-LPDDR4_4GB.png

Then, we load the .ds file to the board via NXP DDR tool.

DDR_tool_information.png

But the information shown in NXP DDR tool is not correct.

The "total DRAM density" should be "8192MB" instead of "4096".

And the "ROW size" should be "17" instead of "16".

If we execute the stress test, the test result shows error:

DDR_tool_stress_test_error.png

 

Is there any way to make 8GB LPDDR4 work on i.mx8M Mini?

 

Thanks~!!!

 

BR,

Richard

 

 

タグ(3)
0 件の賞賛
返信
1 解決策
2,529件の閲覧回数
richard_hu
Senior Contributor I

We get great support from local distributer FAE.

The issue is solved.

I think we can close this thread.

Thanks~!!!

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,530件の閲覧回数
richard_hu
Senior Contributor I

We get great support from local distributer FAE.

The issue is solved.

I think we can close this thread.

Thanks~!!!

0 件の賞賛
返信