NXP i.mx8M Mini with 8GB LPDDR4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP i.mx8M Mini with 8GB LPDDR4

Jump to solution
2,555 Views
richard_hu
Senior Contributor I

Dear, Sir:

We have a custom i.mx8M Mini board.

we have validated 4GB LPDDR4 on it and it works fine.

Now we change the LPDDR4 from 4GB to 8GB. And we encounter some problems.

 

The DDR Register Programming Aid (RPA) we use is "MX8M_Mini_LPDDR4_RPA_v18.xlsx".

The NXP DDR tool we use is "mscale_ddr_tool _v3.20_setup.exe".

 

First, we follow the DRAM datasheet to set up device information for 8GB LPDDR4 in RPA.

i.mx8MM-LPDDR4_4GB.png

Then, we load the .ds file to the board via NXP DDR tool.

DDR_tool_information.png

But the information shown in NXP DDR tool is not correct.

The "total DRAM density" should be "8192MB" instead of "4096".

And the "ROW size" should be "17" instead of "16".

If we execute the stress test, the test result shows error:

DDR_tool_stress_test_error.png

 

Is there any way to make 8GB LPDDR4 work on i.mx8M Mini?

 

Thanks~!!!

 

BR,

Richard

 

 

Tags (3)
0 Kudos
Reply
1 Solution
2,536 Views
richard_hu
Senior Contributor I

We get great support from local distributer FAE.

The issue is solved.

I think we can close this thread.

Thanks~!!!

View solution in original post

0 Kudos
Reply
1 Reply
2,537 Views
richard_hu
Senior Contributor I

We get great support from local distributer FAE.

The issue is solved.

I think we can close this thread.

Thanks~!!!

0 Kudos
Reply