NXP MCU doesnt wake up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP MCU doesnt wake up

Jump to solution
22,075 Views
sapirbuz
Contributor IV

Hi,

 

We have MIMXRT1051CVL5B on our design.

the MCU SNVS and 3.3V rails are in the required range, the clocks are ok, but we can't see a device connected (on the SW or device manager) while we connect the USB host to J16 connector or the NXP debugger to J3 connector.

I have attached our design. Can you please review and let us know what can be the problem?

 

1 Solution
21,720 Views
sapirbuz
Contributor IV
0 Kudos
Reply
15 Replies
22,055 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @sapirbuz ,

  You mentioned the MCU doesn't wake up, do you mean you use the low power mode, or just your customer board can't work? In fact not the low power issues?

  If it is the low power wake up issue, do you also test it on the NXP MIMXRT1050-EVKB, whether that works ok or not? Just make sure your software have no issues.

  You mentioned:  but we can't see a device connected (on the SW or device manager)

Which device? please give me more information about this point, I am a little lost about it.

Best Regards,

Kerry

22,047 Views
sapirbuz
Contributor IV

Hi,

Our board can't work. We connect the USB host or the SWD NXP debugger and nothing happens.

When we connect our board with the NXP to the host, the NXP MCU Boot Utility doesn't recognize the flash, but when we connect the EVKB with the same flash, it is recognized automatically, and we see device connected on the device manager.

sapirbuz_0-1683191844734.png

 

 

22,041 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @sapirbuz ,

   Your board enter the SDP mode failed. Do you set your board in the serial download mode?

   Can you use the debugger enter the debug mode in RAM?

   You can check the SRC status register at first.

    

Best Regards,

Kerry

22,036 Views
sapirbuz
Contributor IV

Do you set your board in the serial download mode?- Yes

   Can you use the debugger enter the debug mode in RAM? no, the debugger isn't recognized as well as the USB.

We noticed that the 3.3V-SNVS and the 3.3V to the other NXP pins raised together.

the 3.3V to the other NXP pins is high before the PMIC_ON_REQ pin is high

    

22,027 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @sapirbuz ,

  Please check two points:

1. POR sequence

kerryzhou_0-1683262627852.png

DCDC_PSWITCH is delayed more than 1ms to switch the internal DCDC on, this is the must.

 

2. Do you have JLINK, you can use the JLINK to check with SWD, whether you can find the M7 core or not?

If the M7 core is not detected, it means your hardware have issues.

Best Regards,

Kerry

 

21,995 Views
sapirbuz
Contributor IV

Hi,

1. DCDC_PSWITCH is delayed 8ms to switch the internal DCDC on.

2. We have SWD debugger, should it work the same as JLINK?

 

Thanks,

Sapir

21,956 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @sapirbuz 

1. DCDC_PSWITCH is delayed 8ms to switch the internal DCDC on.

=>Kerry: it's enough!

2. We have SWD debugger, should it work the same as JLINK?

=>Kerry: SWD is the interface, the JLINK connect interface is SWD, so you can try to use the JLINK connect to the RT board SWD interface, then use the JLINK commander to test it, something like this:

RT1052_JLINK.jpg

JLINK commander can find in the JLINK driver.

 

21,942 Views
sapirbuz
Contributor IV

Hi,

Thank you!

I found the problem in the design: the VDD_USB_CAP is shortened to VDD_SOC_IN.

Can I know if anything may be damaged if the VDD_USB_CAP pin will be float (and not connected to capacitor)

 

 

 

 

21,930 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @sapirbuz ,

  Thanks for your information.

  1. JLINK connection result

     That is not correct, you need to check the SWD connection between your board the JLINK, seems connection have issues.

   If you still have issues, you can share me your connection photo!

2. the USB issues

I don't think your chip is damaged, please remove the VDD_SOC_IN from VDD_USB_CAP.

VDD_USB_CAP should like this:

kerryzhou_0-1683602912081.png

kerryzhou_1-1683602917362.png

 

After the modification, can you find the USB or not in the serial download mode?

Any updated information, kindly let me know.

Best Regards,

kerry

 

21,920 Views
sapirbuz
Contributor IV

Hi,

i don't have the option to connect the VDD_USB_CAP to external capacitors. 

Is that critical? or can the MCU work properly without those capacitors?

21,835 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @sapirbuz ,

 For testing, I think, you need to remove the VDD_SOC_IN from VDD_USB_CAP at first, then try it if you can't add the capacitor. the capacitor is a must if you design the product, but for the simple testing, you can leave it as float at first.

 

Wish it helps you!

Best Regards,

Kerry

21,721 Views
sapirbuz
Contributor IV

ש

0 Kudos
Reply
21,944 Views
sapirbuz
Contributor IV

Hi,

We succeed in connecting the debugger using the MCUXpresso IDE.

The USB is still not recognized.

What can we do to debug the problem using the MCUXpresso IDE?

Should we program something before the USB is recognized? or should it be recognized automatically on a "clean" MCU?

sapirbuz_0-1683559431033.png

 

BDY, the detection failed using the Jlink commander

sapirbuz_1-1683559474775.png

 

22,052 Views
sapirbuz
Contributor IV

Hi,

When we connect our board with the NXP to the host, the NXP MCU Boot Utility doesn't recognize the flash and nothing happens.

But when we connect the EVKB with the same flash, it is recognized automaticall.

sapirbuz_0-1683191393472.png

 

22,050 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @sapirbuz ,

  Seems information is not complete, please give me more information, thanks.

Best Regards,

Kerry