NXP IMX8M Mini LPDDR4 DRAM Calibration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP IMX8M Mini LPDDR4 DRAM Calibration

Jump to solution
4,209 Views
FOC
Contributor I

Hi Everyone,

I would like to ask a simple question. I did a DRAM calibration to the LPDDR4 DRAM on my custom designed imx8m mini board and when I checked the GUI log I didn't see any 'point0@1500MHz' text at the time of stress test. Can you check the file and tell me if there is any problem? I have attached the log file for your reference.

Labels (2)
0 Kudos
Reply
1 Solution
4,154 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Your script seems to be ok and also you are passing the test, I do not see any issues.

These set points are defined on RPA file:

JorgeCas_0-1721140621216.png

Those the values should remain as are and should not be modified. In these cases, the settings are provided for completeness.

Best regards

View solution in original post

0 Kudos
Reply
3 Replies
4,178 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

This is defined on RPA file to generate the script, please verify if point0@1500MHz is included.

Best regards.

0 Kudos
Reply
4,161 Views
FOC
Contributor I

Hi Jorge,

Yes, I think the script includes point0@1500MHz but sorry I am very new to DRAM calibration. I have attached the script I used for your reference.

Regards.

0 Kudos
Reply
4,155 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Your script seems to be ok and also you are passing the test, I do not see any issues.

These set points are defined on RPA file:

JorgeCas_0-1721140621216.png

Those the values should remain as are and should not be modified. In these cases, the settings are provided for completeness.

Best regards

0 Kudos
Reply