Specific HDMI screen resolution 800x480 with i.MX8M-Plus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Specific HDMI screen resolution 800x480 with i.MX8M-Plus

跳至解决方案
179 次查看
JoelWTK
Contributor II

Hello

I'm working with iot-gate-imx8plus from compulab which integrate i.MX8M-Plus CPU and I have difficulties to use a specific screen with resolution 800x480 over HDMI interface.

From the reference manual of the processor, I have read the following:

HDMI 2.0a Tx supporting one display

Resolutions of: 740x480p60, 720x480p60, 1280x720p60, 1920x1080p60, 1920x1080p120, 3840x2160p30

So the resolution I want is not listed. Is it possible to achieve such resolution ?

I started working on the topic by setting a custom edid file, playing with video= kernel parameter to force 800x480 resolution, but still not working. The best I succeed to do is to have HDMI connected and weston complaining because the the HDMI interface has no modes available

Thanks for feedbacks about this topic (I see it has been discussed many times but no clear answer is done).

Joel

0 项奖励
回复
1 解答
35 次查看
JoelWTK
Contributor II
0 项奖励
回复
4 回复数
36 次查看
JoelWTK
Contributor II

Hello,

Problem was HDMY PHY clock values available in linux-imx. See https://community.nxp.com/t5/i-MX-Processors/Specific-HDMI-screen-resolution-quot-hdmi-phy-quot-cloc....

Joel

0 项奖励
回复
151 次查看
JoelWTK
Contributor II

Hello @Bio_TICFSL 

Thanks for the reply. Do you know a tutorial somewhere for that ? Looks not so trivial probably ?

Joel

0 项奖励
回复
150 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Sorry no, the only information about the hdmi driver is on the Linux reference manual

https://www.nxp.com/docs/en/reference-manual/IMX_REFERENCE_MANUAL.pdf

Regards

0 项奖励
回复
154 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The resolution is not supported by the driver, in this case you will have to add it and add it to your dtb.

Regards

0 项奖励
回复