NXP ARM-based processor with Java SE support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP ARM-based processor with Java SE support

4,443件の閲覧回数
stephenades
Contributor I

Hi all

I am looking for a processor that will run Oracle's Java 8 SE for ARM under a flavour of Linux. It looks like a suitable candidate might be an iMX515, but I cannot find a definite statement. Am I right? If not, which NXP processor families will run Java 8 SE?

Thanks

Stephen Ades

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

3,293件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please use the following from Community

All Boards Java

Note, for i.MX6 we should use ARMv7 packages :

Java SE Embedded - Downloads | Oracle Technology Network | Oracle

 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,293件の閲覧回数
stephenades
Contributor I

Hello Yuri.

I don't think that answers my question. All the information you referred to above was about Java SE Embedded. I am interested in Java SE (i.e. the whole JRE). I know that means fitting more memory, but we need it to have the same Java capabilities (including Swing via X windows) as a Java SE application running on an Intel platform has.

If you buy a Raspberry PI (Broadcom ARM Cortex A7 - see Raspberry Pi 2 Model B​) or a CubieTruck (Allwinner ARM Cortex A7) you can run full Java 8 SE and full Java applications on it.

Does NXP have a processor that can run full Java SE?

Regards

Stephen Ades

0 件の賞賛
返信

3,293件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Java is supported under i.MX devices as much as (ARM) Linux and corresponding packages

from Oracle provide it. As I see, Oracle does not provide (full) Java SE for ARM architecture.

Regards,

Yuri.

0 件の賞賛
返信