NVCC_MIPI on 3P3V

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

NVCC_MIPI on 3P3V

跳至解决方案
2,227 次查看
mosmos
Contributor I

On Wandboard and SabreLite NVCC_MIPI is connected to 3P3V.

The datasheet IMX6SDLIEC sets the operating ranges for NVCC_MIPI from 2.25 to 2.75V.

Why is there a difference?

Manuel.

标签 (2)
标记 (5)
0 项奖励
回复
1 解答
2,019 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Manuel

yes your remark is correct: according to

i.MX6Q Datasheet NVCC_MIPI should be from 2.25 to 2.75V.

Please note that these boards are not Freescale boards, so question

should be directed to vendors of these boards.

Though sometimes designers just mark power rail as "3P3V",

really later it can be programmed to other value. I think

this should be investigated on real board.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,020 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Manuel

yes your remark is correct: according to

i.MX6Q Datasheet NVCC_MIPI should be from 2.25 to 2.75V.

Please note that these boards are not Freescale boards, so question

should be directed to vendors of these boards.

Though sometimes designers just mark power rail as "3P3V",

really later it can be programmed to other value. I think

this should be investigated on real board.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复