NVCC_MIPI on 3P3V

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,208件の閲覧回数
mosmos
Contributor I

On Wandboard and SabreLite NVCC_MIPI is connected to 3P3V.

The datasheet IMX6SDLIEC sets the operating ranges for NVCC_MIPI from 2.25 to 2.75V.

Why is there a difference?

Manuel.

ラベル(2)
タグ(5)
0 件の賞賛
返信
1 解決策
2,000件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Manuel

yes your remark is correct: according to

i.MX6Q Datasheet NVCC_MIPI should be from 2.25 to 2.75V.

Please note that these boards are not Freescale boards, so question

should be directed to vendors of these boards.

Though sometimes designers just mark power rail as "3P3V",

really later it can be programmed to other value. I think

this should be investigated on real board.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,001件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Manuel

yes your remark is correct: according to

i.MX6Q Datasheet NVCC_MIPI should be from 2.25 to 2.75V.

Please note that these boards are not Freescale boards, so question

should be directed to vendors of these boards.

Though sometimes designers just mark power rail as "3P3V",

really later it can be programmed to other value. I think

this should be investigated on real board.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信