NAND boot Stride Size Fuse Value

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NAND boot Stride Size Fuse Value

ソリューションへジャンプ
1,843件の閲覧回数
rickardandersso
Contributor IV

The i.MX 6SoloX Applications Processor Reference Manual refers to "Stride Size Fuse Value", but I have searched the reference manual without finding the actual register. Where can I set "Stride Size Fuse Value"?

Thanks,

Rickard

ラベル(1)
1 解決策
1,744件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  The stride size is usually the pages in each block which comes from the

boot configuration (Pages In Block) : “the search area contains copies of the FCB
at each stride distance, so in case the first NAND block becomes corrupted,

the ROM will find its copy in the next NAND block.”

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

元の投稿で解決策を見る

1 返信
1,745件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  The stride size is usually the pages in each block which comes from the

boot configuration (Pages In Block) : “the search area contains copies of the FCB
at each stride distance, so in case the first NAND block becomes corrupted,

the ROM will find its copy in the next NAND block.”

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!