Using PN7150 irq gpio to wake up board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using PN7150 irq gpio to wake up board

2,045件の閲覧回数
pratyushtomar
Contributor IV

I am using PN7150 with custom board based on imx6ul evk. I am using following configuration in dts for PN7150 driver

pn547: pn547@28 {
compatible = "nxp,pn547";
reg = <0x28>;
clock-frequency = <400000>;
interrupt-parent = <&gpio1>;
interrupt-gpios = <&gpio1 30 0>;
enable-gpios = <&gpio1 25 0>;
};

Can I use PN7150 interrupt gpio(gpio 1 30) to wake up my board from sleep at the same time using as PN7150 irq? if yes then how?  I tried adding wake up configuration from interrupt on gpio1 30 in following manner

wakeup1 {
label = "wakeup1 gpio";
gpios = <&gpio1 30 GPIO_ACTIVE_HIGH>;
linux,code = <29>;
gpio-key,wakeup;
};

But after adding this configuration in my dts the PN7150 library doesn't work. The demo program just exits after starting.

ラベル(3)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,461件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Pratyush,

    Try following configuration in your device tree:

wakeup1 {
    label = "wakeup1 gpio";

    interrupt-parent = <&gpio1>;

    interrupts = <30 IRQ_TYPE_LEVEL_HIGH>;

    wakeup-gpios = <&gpio1 30 GPIO_ACTIVE_HIGH>;

};


Have a great day,
TIC Weidong Sun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,461件の閲覧回数
pratyushtomar
Contributor IV

Hello I tried settings mentioned by you in following manner

gpio-keys { /* WAKE UP BOARD */
compatible = "gpio-keys";
wakeup {
label = "wakeup gpio";
gpios = <&gpio4 28 GPIO_ACTIVE_LOW>;
linux,code = <29>;
gpio-key,wakeup;
};
wakeup1 {
label = "wakeup1 gpio";
interrupt-parent = <&gpio1>;
interrupts = <30 IRQ_TYPE_LEVEL_HIGH>;
wakeup-gpios = <&gpio1 30 GPIO_ACTIVE_HIGH>;
};
};

But it's not working. I start my nfcdemoapp and sleep after "waiting for tag" step. Now when I bring tag near nfc the interrupt is generated on gpio1 30. But this doesn't wake up my board. Any suggestion?

0 件の賞賛
返信