NAND Flash - Wait Polarity versus Write Protect

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NAND Flash - Wait Polarity versus Write Protect

ソリューションへジャンプ
2,582件の閲覧回数
atillametetured
Contributor V


Something is puzzling me and would be glad if someone could clear it up. On iMX side NANDF_WP_B pin is described as wait polarity signal. On the NAND flash I have selected, the pin NANDF_WP_B is the hardware write protection pin.

On Sabre AI platform, these two signals are connected so can someone confirm wait polarity and write protection serve the same functionality?

Regards,

Mete

ラベル(1)
タグ(5)
0 件の賞賛
返信
1 解決策
2,282件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mete

it is write protection pin. Description as " wait polarity signal"

was left as gpmi can also work with ata devices (not supported in this chip).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,283件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mete

it is write protection pin. Description as " wait polarity signal"

was left as gpmi can also work with ata devices (not supported in this chip).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,282件の閲覧回数
atillametetured
Contributor V

Hi Igor,

Thank you for the information.

Best Regards,

Mete

0 件の賞賛
返信