NAND Flash - Wait Polarity versus Write Protect

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NAND Flash - Wait Polarity versus Write Protect

Jump to solution
2,586 Views
atillametetured
Contributor V


Something is puzzling me and would be glad if someone could clear it up. On iMX side NANDF_WP_B pin is described as wait polarity signal. On the NAND flash I have selected, the pin NANDF_WP_B is the hardware write protection pin.

On Sabre AI platform, these two signals are connected so can someone confirm wait polarity and write protection serve the same functionality?

Regards,

Mete

Labels (1)
Tags (5)
0 Kudos
Reply
1 Solution
2,286 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mete

it is write protection pin. Description as " wait polarity signal"

was left as gpmi can also work with ata devices (not supported in this chip).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
2,287 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mete

it is write protection pin. Description as " wait polarity signal"

was left as gpmi can also work with ata devices (not supported in this chip).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,286 Views
atillametetured
Contributor V

Hi Igor,

Thank you for the information.

Best Regards,

Mete

0 Kudos
Reply