NAND Flash - Wait Polarity versus Write Protect

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

NAND Flash - Wait Polarity versus Write Protect

跳至解决方案
2,580 次查看
atillametetured
Contributor V


Something is puzzling me and would be glad if someone could clear it up. On iMX side NANDF_WP_B pin is described as wait polarity signal. On the NAND flash I have selected, the pin NANDF_WP_B is the hardware write protection pin.

On Sabre AI platform, these two signals are connected so can someone confirm wait polarity and write protection serve the same functionality?

Regards,

Mete

标签 (1)
标记 (5)
0 项奖励
回复
1 解答
2,280 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mete

it is write protection pin. Description as " wait polarity signal"

was left as gpmi can also work with ata devices (not supported in this chip).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
2,281 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mete

it is write protection pin. Description as " wait polarity signal"

was left as gpmi can also work with ata devices (not supported in this chip).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,280 次查看
atillametetured
Contributor V

Hi Igor,

Thank you for the information.

Best Regards,

Mete

0 项奖励
回复