We are discussing a project which may need two 1080P displays,HDMI and LVDS.About these two interface,we have experience in using it on IMX6Q in previous project.Now we want to use it at the same time.
So I want to known if the IMX6Q chip can support two 1080P displays at the same time? If support,it can operate at which temperature without cooling device?
已解决! 转到解答。
Hi 千 浪 .
yes, it is supported without problems.
Regarding temperature without cooling one can look at
AN4579 i.MX 6 Series Thermal Management Guidelines"
http://www.freescale.com/files/32bit/doc/app_note/AN4579.pdf
Best regards
igor
Hi 千 浪 .
yes, it is supported without problems.
Regarding temperature without cooling one can look at
AN4579 i.MX 6 Series Thermal Management Guidelines"
http://www.freescale.com/files/32bit/doc/app_note/AN4579.pdf
Best regards
igor