Multi-displays

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,749件の閲覧回数
thouswave
Contributor III

We are discussing a project which may need two 1080P displays,HDMI and LVDS.About these two interface,we have experience in using it on IMX6Q in previous project.Now we want to use it at the same time.

So I want to known if the IMX6Q chip can support two 1080P displays at the same time? If support,it can operate at which temperature without cooling device?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,629件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 千 浪 .

yes, it is supported without problems.

Regarding temperature without cooling one can look at

AN4579 i.MX 6 Series Thermal Management Guidelines"

http://www.freescale.com/files/32bit/doc/app_note/AN4579.pdf

Best regards

igor

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,630件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 千 浪 .

yes, it is supported without problems.

Regarding temperature without cooling one can look at

AN4579 i.MX 6 Series Thermal Management Guidelines"

http://www.freescale.com/files/32bit/doc/app_note/AN4579.pdf

Best regards

igor

0 件の賞賛
返信