Minimal resolution on LVDS, iMX6S

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Minimal resolution on LVDS, iMX6S

跳至解决方案
2,333 次查看
cerma
Contributor IV

Hello, what is minimal resolution on LVDS? I saw in datasheet that minimal frequency is 0 - 85 MHz but there was also mentioned that minimal frequency is 25 MHz. I need to set 480x272 (frequency about 9 MHz) but I don't know if is that even possible. Is it possible to set this resolution, if so, how?

0 项奖励
回复
1 解答
1,698 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Jaroslav,

     9MHz should be no problem, one of our customers set (320X240) 6.4MHz with LVDS1 port successfully, please refer to the following steps and adjust your source code :

(1)ldb.c ( configuring your LCD's timg according to LCD's datasheet)

static struct fb_videomode ldb_modedb[] = {
{
"LDB-XGA", 60, 320, 240, 155914,
38, 20,
15, 4,
30, 3,
0,
FB_VMODE_NONINTERLACED,
FB_MODE_IS_DETAILED,},

(2)Adjusting clock source code in /arch/arm/mach-mx6/clock.c

Find :

clk_set_parent(&ldb_di0_clk, &pll2_pfd_352M);

       clk_set_parent(&ldb_di1_clk, &pll2_pfd_352M);

and change it to be:

clk_set_parent(&ldb_di0_clk, &pll5_video_main_clk,);

       clk_set_parent(&ldb_di1_clk, &pll5_video_main_clk,);


(3)BSP file: mach-mx6q/board-mx6q_sasbresd.c

static struct ipuv3_fb_platform_data sabresd_fb_data[] = {

            { /*fb0*/

            .disp_dev = "ldb",

            .interface_pix_fmt = IPU_PIX_FMT_RGB666,

            .mode_str = "LDB-XGA",

            .default_bpp = 16,

            .int_clk = false,

            .late_init = false,

"int_clk = false" means the clock source is from PLL2_PFD_352 or pll5_video_main_clk  ; "int_clk = true" means clock source is from IPU(264MHz)



Hope the above advice can help you !


--------------------------------

If above suggestion can help you resolve your issue, please help close the post !

--------------------------------

Regards,

Weidong

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,699 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Jaroslav,

     9MHz should be no problem, one of our customers set (320X240) 6.4MHz with LVDS1 port successfully, please refer to the following steps and adjust your source code :

(1)ldb.c ( configuring your LCD's timg according to LCD's datasheet)

static struct fb_videomode ldb_modedb[] = {
{
"LDB-XGA", 60, 320, 240, 155914,
38, 20,
15, 4,
30, 3,
0,
FB_VMODE_NONINTERLACED,
FB_MODE_IS_DETAILED,},

(2)Adjusting clock source code in /arch/arm/mach-mx6/clock.c

Find :

clk_set_parent(&ldb_di0_clk, &pll2_pfd_352M);

       clk_set_parent(&ldb_di1_clk, &pll2_pfd_352M);

and change it to be:

clk_set_parent(&ldb_di0_clk, &pll5_video_main_clk,);

       clk_set_parent(&ldb_di1_clk, &pll5_video_main_clk,);


(3)BSP file: mach-mx6q/board-mx6q_sasbresd.c

static struct ipuv3_fb_platform_data sabresd_fb_data[] = {

            { /*fb0*/

            .disp_dev = "ldb",

            .interface_pix_fmt = IPU_PIX_FMT_RGB666,

            .mode_str = "LDB-XGA",

            .default_bpp = 16,

            .int_clk = false,

            .late_init = false,

"int_clk = false" means the clock source is from PLL2_PFD_352 or pll5_video_main_clk  ; "int_clk = true" means clock source is from IPU(264MHz)



Hope the above advice can help you !


--------------------------------

If above suggestion can help you resolve your issue, please help close the post !

--------------------------------

Regards,

Weidong

0 项奖励
回复
1,698 次查看
haitao
Contributor II

你好,weidong!

按照你的方法,我得到的时钟最低为25.6M,我得不到9M的时钟。不知道为什么

0 项奖励
回复