Minimal resolution on LVDS, iMX6S

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Minimal resolution on LVDS, iMX6S

ソリューションへジャンプ
2,331件の閲覧回数
cerma
Contributor IV

Hello, what is minimal resolution on LVDS? I saw in datasheet that minimal frequency is 0 - 85 MHz but there was also mentioned that minimal frequency is 25 MHz. I need to set 480x272 (frequency about 9 MHz) but I don't know if is that even possible. Is it possible to set this resolution, if so, how?

0 件の賞賛
返信
1 解決策
1,696件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Jaroslav,

     9MHz should be no problem, one of our customers set (320X240) 6.4MHz with LVDS1 port successfully, please refer to the following steps and adjust your source code :

(1)ldb.c ( configuring your LCD's timg according to LCD's datasheet)

static struct fb_videomode ldb_modedb[] = {
{
"LDB-XGA", 60, 320, 240, 155914,
38, 20,
15, 4,
30, 3,
0,
FB_VMODE_NONINTERLACED,
FB_MODE_IS_DETAILED,},

(2)Adjusting clock source code in /arch/arm/mach-mx6/clock.c

Find :

clk_set_parent(&ldb_di0_clk, &pll2_pfd_352M);

       clk_set_parent(&ldb_di1_clk, &pll2_pfd_352M);

and change it to be:

clk_set_parent(&ldb_di0_clk, &pll5_video_main_clk,);

       clk_set_parent(&ldb_di1_clk, &pll5_video_main_clk,);


(3)BSP file: mach-mx6q/board-mx6q_sasbresd.c

static struct ipuv3_fb_platform_data sabresd_fb_data[] = {

            { /*fb0*/

            .disp_dev = "ldb",

            .interface_pix_fmt = IPU_PIX_FMT_RGB666,

            .mode_str = "LDB-XGA",

            .default_bpp = 16,

            .int_clk = false,

            .late_init = false,

"int_clk = false" means the clock source is from PLL2_PFD_352 or pll5_video_main_clk  ; "int_clk = true" means clock source is from IPU(264MHz)



Hope the above advice can help you !


--------------------------------

If above suggestion can help you resolve your issue, please help close the post !

--------------------------------

Regards,

Weidong

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,697件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Jaroslav,

     9MHz should be no problem, one of our customers set (320X240) 6.4MHz with LVDS1 port successfully, please refer to the following steps and adjust your source code :

(1)ldb.c ( configuring your LCD's timg according to LCD's datasheet)

static struct fb_videomode ldb_modedb[] = {
{
"LDB-XGA", 60, 320, 240, 155914,
38, 20,
15, 4,
30, 3,
0,
FB_VMODE_NONINTERLACED,
FB_MODE_IS_DETAILED,},

(2)Adjusting clock source code in /arch/arm/mach-mx6/clock.c

Find :

clk_set_parent(&ldb_di0_clk, &pll2_pfd_352M);

       clk_set_parent(&ldb_di1_clk, &pll2_pfd_352M);

and change it to be:

clk_set_parent(&ldb_di0_clk, &pll5_video_main_clk,);

       clk_set_parent(&ldb_di1_clk, &pll5_video_main_clk,);


(3)BSP file: mach-mx6q/board-mx6q_sasbresd.c

static struct ipuv3_fb_platform_data sabresd_fb_data[] = {

            { /*fb0*/

            .disp_dev = "ldb",

            .interface_pix_fmt = IPU_PIX_FMT_RGB666,

            .mode_str = "LDB-XGA",

            .default_bpp = 16,

            .int_clk = false,

            .late_init = false,

"int_clk = false" means the clock source is from PLL2_PFD_352 or pll5_video_main_clk  ; "int_clk = true" means clock source is from IPU(264MHz)



Hope the above advice can help you !


--------------------------------

If above suggestion can help you resolve your issue, please help close the post !

--------------------------------

Regards,

Weidong

0 件の賞賛
返信
1,696件の閲覧回数
haitao
Contributor II

你好,weidong!

按照你的方法,我得到的时钟最低为25.6M,我得不到9M的时钟。不知道为什么

0 件の賞賛
返信