Mfgtool flashing issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mfgtool flashing issue

ソリューションへジャンプ
4,107件の閲覧回数
manjunathjoshi
Contributor V

Hello all,

I am seeing a tar error at the very end of a flash which i am attaching. Can anybody guess what's the exact issue?

Has anybody got similar issue ? Please let me know as soon as possible.

Regards,

Manju

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
3,902件の閲覧回数
manjunathjoshi
Contributor V

Hello All,

This issue was solved when i renamed rootfs.tar.bz2 to rootfs.tar.

This is a work around but surely worked for me.

Regards,

Manju

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,902件の閲覧回数
b36401
NXP Employee
NXP Employee

The error itself (invalid tar magic) means that tar does not find archive signature.

It may be caused with damaged image.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,902件の閲覧回数
manjunathjoshi
Contributor V

Hello victor,

The same image is untarred in many other boards. That's the tricky part.

I want to know when such error might occur? Not one instance of it.

Regards,

Manju

0 件の賞賛
返信
3,903件の閲覧回数
manjunathjoshi
Contributor V

Hello All,

This issue was solved when i renamed rootfs.tar.bz2 to rootfs.tar.

This is a work around but surely worked for me.

Regards,

Manju

0 件の賞賛
返信