MfgTool for Windows and vmware for iMX28

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MfgTool for Windows and vmware for iMX28

2,734 次查看
bfod
Contributor I

Is it possible to use MfgTool for Windows on a VMWARE virtual machine?

It fails after "Booting update client engine"

MfgTool version v1.6.2.048

Where can i find the 055 release?

标签 (2)
0 项奖励
回复
3 回复数

2,099 次查看
bfod
Contributor I

Thx for the swift reply,

This file contains the source code, where can i find the "exe" file?

Any experience with virtual machine like VMWare?

0 项奖励
回复

2,099 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复

2,099 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Marc

for 055 release please check

Programmers (Flash, etc.) (3)

IMX_MFG_TOOL_SOURCE  : Source Code for the i.MX manufacturing tool used
for downloading OS images to the i.MX53, i.MX51, i.MX50, i.MX28 and i.MX23..
Size (K): 1226 Format: zip Rev #: 1.6.2.055 Modified: 7/22/2013

http://www.nxp.com/products/power-management/pmics/power-management-for-i.mx-application-processors/...

Best regards
igor

0 项奖励
回复