PMIC PF3000 RESETBMCU signal

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PMIC PF3000 RESETBMCU signal

1,451 次查看
marklu
Contributor II

Hi

Based on PF3000 datasheet, page31(6.3.1.3) show "In the default mode, the RESETBMCU signal is internal timer based and does not monitor the regulators". Do it mean if we connect RESETBMCU to i.MX6, we can't guarantee the reset signal will be applied after each power is delivered well (power good).

If we want to deliver reset signal to CPU after each power is good, it seems PMIC will go to fault mode instead of default mode. Do we set OTP_PG_EN to 1 to achieve it? If we already set it once, do it also keep modified value for next power cycle (power on/off)?

BRs

Mark

标签 (2)
0 项奖励
回复
1 回复

1,251 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mark

>Do it mean if we connect RESETBMCU to i.MX6, we can't guarantee the reset signal

>will be applied after each power is delivered well (power good).

yes

>Do we set OTP_PG_EN to 1 to achieve it?

yes

>If we already set it once, do it also keep modified value for next power cycle (power on/off)?

yes

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------