Message Queues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Message Queues

3,459 Views
jpe1313
Contributor II

I'm using the Yocto Freescale   core-image-base on the SABRE i.MX6 QUAD evaluation board.

I'd like to use message queues but they don't seem to be supported in this kernel?   Is that true or am I missing something?

THANKS IN ADVANCE

Labels (3)
3 Replies

3,064 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Janet Estabridis,

If you are referring to POSIX message queues these are not enabled by default, but you may use menuconfig to enable this function under General Setup > POSIX Message Queues.

There is more information on how to configure the kernel on the following document, which I'm sure will be very helpful.

https://community.nxp.com/docs/DOC-94196 

Regards,

0 Kudos
Reply

3,064 Views
jpe1313
Contributor II

When I click on the link it says

Unauthorized


Access to this place or content is restricted. If you think this is a mistake, please contact your administrator or the person who directed you here.
CAN YOU HELP ME OUT?  I really want to enable the POSIX message queues and I've never recompiled a kernel for NXP.
Thanks
0 Kudos
Reply

3,064 Views
gusarambula
NXP TechSupport
NXP TechSupport

My apologies. Try this link instead:

https://community.nxp.com/docs/DOC-95045