adv7280m scrolled video

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

adv7280m scrolled video

Jump to solution
1,147 Views
kurkinalexandr
Contributor III

Hi All.

I was able to capture video, using Adv7280m and imx6.  But video is being scrolled up.  It isn`t depend on if I receive test pattern or capture real video from a camera. In both cases I get being scrolled vertically video. So most likely I have imx6 configuration issue.

My sensor pass 480p mipi csi data on 216Mbps . I don`t have any errors on mipi csi2 dphy level(status = 0x300)

But each time I get warning:

<4>imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00000001

I fond that Yury Kocherov had the similar problem in this branch https://community.nxp.com/message/812742?commentID=812742#comment-812742 .

Did anybody meet similar issue and can get advice?

0 Kudos
1 Solution
603 Views
kurkinalexandr
Contributor III

The reason - wrong vertical frame size. In autodetect mode the Adv7280m sends 480p frames. No matter what the camera is connected: Pal or Ntsc(didn`t test secam) - in my case the decoder sent 480p in autodetect mode.

View solution in original post

0 Kudos
2 Replies
604 Views
kurkinalexandr
Contributor III

The reason - wrong vertical frame size. In autodetect mode the Adv7280m sends 480p frames. No matter what the camera is connected: Pal or Ntsc(didn`t test secam) - in my case the decoder sent 480p in autodetect mode.

0 Kudos
603 Views
igorpadykov
NXP Employee
NXP Employee

Hi Fan

one can check:

1. the adv7280 should be enabled after mipi_csi2_reset().

2. For MIPI CSI input, the clock mode in IPU_CSI_SENS_CONF must be gated clock mode.

          p->u.bt656.clock_curr = 1;

3. For interlaced input, IDMAC 0 should be set to interlaced mode: "params.csi_mem.interlaced = true;" For progressive input, IDMAC 0 shoudl be set to progressive mode: "params.csi_mem.interlaced = false;"

          case IPU_CSI_CLK_MODE_GATED_CLK: in file drivers\media\video\mxc\capture\ipu_csi_enc.c, function csi_enc_setup().

4. For device type:

     adv7280_data.sen.pix.priv = 1;  /* 1 is used to indicate TV in */

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos