Max output curret of i.MX6ULL internal LDOs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Max output curret of i.MX6ULL internal LDOs

跳至解决方案
1,683 次查看
mamorukanou
Contributor IV

Hi community,

 

The IMX has two built-in LDOs (LDO_ARM, LDO_SOC).

Please let me know the maximum output current of each LDO.

We are trying to do PI analysis on our board, but I need this parameter.

BR,

kanou

mamorukanou_0-1620804347450.png

 

标签 (1)
0 项奖励
回复
1 解答
1,663 次查看
art
NXP Employee
NXP Employee

The maximum load current of both LDO_ARM and LDO_SOC regulators of the i.MX6ULL processor is 250mA.

Best Regards,
Artur

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,664 次查看
art
NXP Employee
NXP Employee

The maximum load current of both LDO_ARM and LDO_SOC regulators of the i.MX6ULL processor is 250mA.

Best Regards,
Artur

0 项奖励
回复
1,679 次查看
mamorukanou
Contributor IV

PS: i.MX is i.MX6UL or 6ULL.

0 项奖励
回复