Max output curret of i.MX6ULL internal LDOs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Max output curret of i.MX6ULL internal LDOs

Jump to solution
1,751 Views
mamorukanou
Contributor IV

Hi community,

 

The IMX has two built-in LDOs (LDO_ARM, LDO_SOC).

Please let me know the maximum output current of each LDO.

We are trying to do PI analysis on our board, but I need this parameter.

BR,

kanou

mamorukanou_0-1620804347450.png

 

Labels (1)
0 Kudos
Reply
1 Solution
1,731 Views
art
NXP Employee
NXP Employee

The maximum load current of both LDO_ARM and LDO_SOC regulators of the i.MX6ULL processor is 250mA.

Best Regards,
Artur

View solution in original post

0 Kudos
Reply
2 Replies
1,732 Views
art
NXP Employee
NXP Employee

The maximum load current of both LDO_ARM and LDO_SOC regulators of the i.MX6ULL processor is 250mA.

Best Regards,
Artur

0 Kudos
Reply
1,747 Views
mamorukanou
Contributor IV

PS: i.MX is i.MX6UL or 6ULL.

0 Kudos
Reply