MXCFB_WAIT_FOR_VSYNC: timeout

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MXCFB_WAIT_FOR_VSYNC: timeout

ソリューションへジャンプ
3,065件の閲覧回数
kevincheng
Contributor IV

Hi,

 

Sometime we power-on the device. LVDS panel is black and no infomation on LVDS panel.

Check the dmesg, there've "MXCFB_WAIT_FOR_VSYNC: timeout" message always repeate.

We've already disable "CONFIG_MX6_CLK_FOR_BOOTUI_TRANS" in kernel , but it seems no help.

Have any method to solve this problem ?  Thanks!!

 

My enviroemnt,

CPU : imx6Q

Memory : 2GB

Output display : LVDS & HDMI

OS : Android 4.3

Base on BSP: android_jb4.3_1.1.1

 

 

 

Regards,

Kevin

Original Attachment has been moved to: vsync_timeout.txt.zip

ラベル(3)
1 解決策
2,360件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Kevin

similar issue was described in

imx6 android 4.3.1 IPU error when system start

so one can follow suggestion given at "24.06.2014 2:00",

note, "fb0base" is also defined in uboot/include/configs/mx6solo_sabresd_android.h

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,361件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Kevin

similar issue was described in

imx6 android 4.3.1 IPU error when system start

so one can follow suggestion given at "24.06.2014 2:00",

note, "fb0base" is also defined in uboot/include/configs/mx6solo_sabresd_android.h

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------