MXCFB_WAIT_FOR_VSYNC: timeout

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MXCFB_WAIT_FOR_VSYNC: timeout

Jump to solution
3,062 Views
kevincheng
Contributor IV

Hi,

 

Sometime we power-on the device. LVDS panel is black and no infomation on LVDS panel.

Check the dmesg, there've "MXCFB_WAIT_FOR_VSYNC: timeout" message always repeate.

We've already disable "CONFIG_MX6_CLK_FOR_BOOTUI_TRANS" in kernel , but it seems no help.

Have any method to solve this problem ?  Thanks!!

 

My enviroemnt,

CPU : imx6Q

Memory : 2GB

Output display : LVDS & HDMI

OS : Android 4.3

Base on BSP: android_jb4.3_1.1.1

 

 

 

Regards,

Kevin

Original Attachment has been moved to: vsync_timeout.txt.zip

Labels (3)
1 Solution
2,357 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kevin

similar issue was described in

imx6 android 4.3.1 IPU error when system start

so one can follow suggestion given at "24.06.2014 2:00",

note, "fb0base" is also defined in uboot/include/configs/mx6solo_sabresd_android.h

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
2,358 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kevin

similar issue was described in

imx6 android 4.3.1 IPU error when system start

so one can follow suggestion given at "24.06.2014 2:00",

note, "fb0base" is also defined in uboot/include/configs/mx6solo_sabresd_android.h

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------