MXCFB_WAIT_FOR_VSYNC: timeout

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MXCFB_WAIT_FOR_VSYNC: timeout

跳至解决方案
3,046 次查看
kevincheng
Contributor IV

Hi,

 

Sometime we power-on the device. LVDS panel is black and no infomation on LVDS panel.

Check the dmesg, there've "MXCFB_WAIT_FOR_VSYNC: timeout" message always repeate.

We've already disable "CONFIG_MX6_CLK_FOR_BOOTUI_TRANS" in kernel , but it seems no help.

Have any method to solve this problem ?  Thanks!!

 

My enviroemnt,

CPU : imx6Q

Memory : 2GB

Output display : LVDS & HDMI

OS : Android 4.3

Base on BSP: android_jb4.3_1.1.1

 

 

 

Regards,

Kevin

Original Attachment has been moved to: vsync_timeout.txt.zip

标签 (3)
1 解答
2,341 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Kevin

similar issue was described in

imx6 android 4.3.1 IPU error when system start

so one can follow suggestion given at "24.06.2014 2:00",

note, "fb0base" is also defined in uboot/include/configs/mx6solo_sabresd_android.h

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
2,342 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Kevin

similar issue was described in

imx6 android 4.3.1 IPU error when system start

so one can follow suggestion given at "24.06.2014 2:00",

note, "fb0base" is also defined in uboot/include/configs/mx6solo_sabresd_android.h

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------