MX7 JTAG Interface pullup/down

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX7 JTAG Interface pullup/down

Jump to solution
1,957 Views
demoniacmilk
Contributor IV

Hello!

The MX7 datasheet states that no external pullups/downs are required on JTAG but if desired pullups of ~10k may be used (except on TDO and MODE).
The reference design ha pullups on TDS and TDI. Not on TCK. Whats the benefit of adding the pullups? And why was none added on the TCK line?

Thank you.

Labels (2)
0 Kudos
Reply
1 Solution
1,831 Views
igorpadykov
NXP Employee
NXP Employee

Hi Lars

weak resistors make signal susceptible to noise, so

based on specific board design additional pull resistors may be added

for improving board noise resistance.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,832 Views
igorpadykov
NXP Employee
NXP Employee

Hi Lars

weak resistors make signal susceptible to noise, so

based on specific board design additional pull resistors may be added

for improving board noise resistance.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply