MMPF0100 power-down sequence when enters OFF mode.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMPF0100 power-down sequence when enters OFF mode.

Jump to solution
1,631 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about MMPF0100.

You know in OFF mode, MMPF0100 stops all power outputs except VCOREDIG and VSNVS.

I want to know the power-down sequence of MMPF0100 outputs when MMPF0100 enters in OFF.

Would you let me know it?

Best Regards,

Satoshi Shimoda

Tags (1)
0 Kudos
Reply
1 Solution
1,530 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

MMPF0100  datasheet does not specify power-down sequence,

that means that sequencer is not used at power-down and one can

think that outputs are turned off simultaneously.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,531 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

MMPF0100  datasheet does not specify power-down sequence,

that means that sequencer is not used at power-down and one can

think that outputs are turned off simultaneously.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply