Is there a flag in the I.MX6 that signals when an EEPROM Recovery boot is performed?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a flag in the I.MX6 that signals when an EEPROM Recovery boot is performed?

962件の閲覧回数
andrelabelle
Contributor I

Hi,

I have my fuses programmed to boot from SD and I also have the EEPROM Recovery bit set.

U-Boot is on both the SD card and the SPI-NOR flash.

Normally the system boots from the SD. If I wipe U-Boot from the SD the system boots from SPI-NOR.

So my question is: Once the I.MX6 is booted from SPI-NOR, is there any way for it to detect that it has booted from SPI-NOR and not the SD card?

Thanks,

Andre

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

866件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi andre

there is no such flag for recovery.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信