MMPF0100 power-down sequence when enters OFF mode.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMPF0100 power-down sequence when enters OFF mode.

ソリューションへジャンプ
1,635件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about MMPF0100.

You know in OFF mode, MMPF0100 stops all power outputs except VCOREDIG and VSNVS.

I want to know the power-down sequence of MMPF0100 outputs when MMPF0100 enters in OFF.

Would you let me know it?

Best Regards,

Satoshi Shimoda

タグ(1)
0 件の賞賛
返信
1 解決策
1,534件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

MMPF0100  datasheet does not specify power-down sequence,

that means that sequencer is not used at power-down and one can

think that outputs are turned off simultaneously.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,535件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

MMPF0100  datasheet does not specify power-down sequence,

that means that sequencer is not used at power-down and one can

think that outputs are turned off simultaneously.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信