MMPF0100 VGEN4 1.8V

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MMPF0100 VGEN4 1.8V

跳至解决方案
1,264 次查看
sylvia
Contributor I

Hi Community

We had received Default Configuration of MMPF0100, The default voltage at VGEN4 is not got. All other regulator outputs are proper.

Kindly suggest what may be the issue. The  input to PMIC (VIN) is 3.4V. If suppose we power up the PMIC through Battery , the input Voltage will go upto 4.2 V.

Is there any proplem for the regulators, since VGEN4 Input regulator VIN max is 3.6 V???

Thanks and Regards

Sylvia

标记 (1)
0 项奖励
回复
1 解答
1,126 次查看
Yuri
NXP Employee
NXP Employee

  Please check Your design regarding the Startup erratum

(False start and/or non-start of regulators).

http://cache.freescale.com/files/analog/doc/errata/MMPF0100ZER.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,127 次查看
Yuri
NXP Employee
NXP Employee

  Please check Your design regarding the Startup erratum

(False start and/or non-start of regulators).

http://cache.freescale.com/files/analog/doc/errata/MMPF0100ZER.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复