MMPF0100 VGEN4 1.8V

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,767件の閲覧回数
sylvia
Contributor I

Hi Community

We had received Default Configuration of MMPF0100, The default voltage at VGEN4 is not got. All other regulator outputs are proper.

Kindly suggest what may be the issue. The  input to PMIC (VIN) is 3.4V. If suppose we power up the PMIC through Battery , the input Voltage will go upto 4.2 V.

Is there any proplem for the regulators, since VGEN4 Input regulator VIN max is 3.6 V???

Thanks and Regards

Sylvia

タグ(1)
0 件の賞賛
返信
1 解決策
1,629件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Please check Your design regarding the Startup erratum

(False start and/or non-start of regulators).

http://cache.freescale.com/files/analog/doc/errata/MMPF0100ZER.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,630件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Please check Your design regarding the Startup erratum

(False start and/or non-start of regulators).

http://cache.freescale.com/files/analog/doc/errata/MMPF0100ZER.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信