Hi,
I want to interface Sony LVDS camera to i.MX 8Q MAX processor. I want to use Lattice Crosslink ( D-PHY Revision 1.1 ) device as bridge for LVDS to MIPI-CSI2 conversion. The Crosslink D-PHY is 1.2V versus i.MX8M 1.0V.
My question is can I use the Crosslink device without any issue ?
BR,
Sameer
Hi Joan,
Thanks. I had asked Lattice already. They think it should work. The VIH and VIL levels for the Crosslink device MIPI D-PHY are as follows, ( MIN, TYP, MAX)
BR,
Sameer