MIPI -CSI2 Interface with i.MX8QM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIPI -CSI2 Interface with i.MX8QM

1,671 Views
sameer_pitre
Contributor II

Hi,

I want to interface Sony LVDS camera to i.MX 8Q MAX processor. I want to use Lattice Crosslink ( D-PHY Revision 1.1 ) device as bridge for LVDS to MIPI-CSI2 conversion. The Crosslink D-PHY is 1.2V versus i.MX8M 1.0V.

My question is can I use the Crosslink device without any issue ?

BR,

Sameer

 

2 Replies

1,511 Views
joanxie
NXP TechSupport
NXP TechSupport

it is likely to work, but would recommend asking Lattice to comment on the different operating voltage conditions to be sure.

1,511 Views
sameer_pitre
Contributor II

Hi Joan,

Thanks. I had asked Lattice already. They think it should work. The VIH and VIL levels for the Crosslink device MIPI D-PHY are as follows, ( MIN, TYP, MAX)

pastedImage_1.png

BR,

Sameer

0 Kudos
Reply